Condensing temperature

The condensing temperature is the temperature at which a cooling medium changes phases from a gas to a liquid.

The condensing temperature is the temperature at which a cooling medium changes phases from a gas to a liquid. When this phase change occurs, the cooling medium condenses. The temperature at which a cooling medium condenses is dependent on the type of coolant and the condensing pressure.

The diagram shows the position of the condenser in a cooling system.





    Facebook Twitter LinkedIn Technorati