Drip/Micro Spray

Overview

Overview

Drip and micro-spray irrigation are for low pressure applications, where there is a requirement for reducing potential evaporation and run off as much as possible. Keeping the pressure constant is vital for ensuring uniform application throughout each zone in the system, and this can be the most energy-efficient method of irrigation, if managed properly. Achieving this requires that the system can compensate for the variations in flow to ensure constant pressure, as zones cut in and out.

A variable speed pump ensures constant pressure in the zones, while keeping operating costs down at the same time. The pump control connected to Grundfos pumps can also monitor the pump data, and this can be used to detect when the sand filter needs cleaning. In precision irrigation systems, Grundfos can also integrate chemical injection equipment that ensures a uniform mix in the line.





    Facebook Twitter LinkedIn Technorati
Contact
Local Sales companies

Telephone

1300 337 733

Fax

1300 782 080

Address

HEAD OFFICE
515 South Road
Regency Park
SA 5010

Local service centre